Hi,
I am doing a university project and my group are trying to create a tension torsion test machine to work inside an SEM, we would like the option to control with torque and position and we were hoping you could recommend a motor, drive and interface for us that would be suitable for this application. We would be looking at a controlled torque of less than 0.5Nm~70oz-in and a total size of the machine being 100x100x25mm~3.9" x 3.9" x 1", so we need to be mindful of size when considering the need for a linear motor and a heater too. For the control loop, we were thinking of an optical encoder for both position and torque.
Any advice and recommendations on different products would be appreciated.