Hello,
from time to time you can find some cries for help like:
“I have bought xxxx and it does not work”
Without any other information. It is fully normal that a beginner or
someone else have a problem with the new toy. But it is a hard work
to get all the needed information to solve the problem.
If you want to speedup the procedure, some more information is needed.
To solve a hardware problem some information like the following is needed:
- 
which target cpu is used, like STR710, LPC2148 and so on
 - 
which jtag hardware is used
 - 
if you could provide the schematics, this could be helped,
 
perhaps you have a link on it.
If you have trouble with a special evaluation board, do you have an other
one and could reproduce the problem too. Perhaps the problem does not exist
here. This information could help to solve the problem.
If you have trouble with some software. It is not helpful like:
“My compiler is not working”
Here it is helpful to provide the version information of the compiler.
Or some small example to reproduce the problem.
Thinking about the following. You have create a new product. Someone bought
it, and you get only the information: “Your product is not working”.
Now you have the same problem, you want to help, but could not.
You need more input.
Does anyone have an idea for a checklist or something else which could help
to solve the problem? Perhaps we can collect some basics which are needed
and make the topic sticky?
Best regards,
Michael