Arduino and Sparkfun AVR Programmer
Running Arduino IDE 1.8.3, Windows 7 Professional. Using the Sparkfun tiny programmer to program the ATtiny85 chip. Have no Issues at all programming the ATtiny85, However when I try the ATtiny45, I have nothing but trouble just using the simple blink LED program. Using the ATtiny45 get 90% verify errors, and then sometimes it will actually verify. On the ATtiny85 I have no issues at all using the exact same program. The chip is mounted in the socket on the Tiny Programmer and connected to no other circuit. It is driving me nuts. The chips are the same except for memory size.
Thank you very much
Darryl…