Hello Sparkfun Forum,
A device to drop a parachute from a kite has been developed successfully. It uses a 433mhz transceiver to
signal a miniature Arduino device, a Beetle DFRobot to operate a servo.
The transceiver is by Rodot.
https://www.amazon.com/dp/B099YXFZGT?re … tails&th=1
Mini Relay Wireless Switch, 433Mhz Remote Control Relay Switch, 984FT Long Range,
DC 6V 12V 24V 1CH Channel Relay Wireless Secure RF Transmitter and Receiver kit, Momentary Toggle Latched Mode
Visit the RODOT Store
The Rodot transceiver range is about 60 meters when up in the air. A range of at least 100 meters is sought.
A transceiver by BSWW was installed and does not work reliably.
This a YouTube video of a demo of the Rodot transceiver.
https://www.youtube.com/shorts/vSckQReVgyU
This a schematic of the operating transceiver to servo.
https://www.kitemessenger.net/Kite_Mess … 211118.jpg
The BSWW transceiver does not work so transceiver with a longer range is sought.
Have found devices like
RFM69HCW Wireless Transceiver - 915MHz
In stock COM-13909 ROHS
and
TI CC1101 Wireless 868Mhz 915Mhz RF Module Long Range 1.5km IPEX/Stamp Hole Antenna
SMD Package E07-900M10S SPI Wireless Module
But these seem to be the receiver without a transmitter.
Can these receivers be paired with a tranmitter? If so where are the transmitters available?
Thanks.
Allen in Dallas