Trimble IQ to PIC16F627A

I wrote a program to read NMEA data into the onboard USART. I begin by sending a factory reset command to the IQ module then try to read one character into the uP but I get a framing error. I initialize the USART to transmit at 9600 baud and receive at 4800 baud . I purchased a SPARK FUN IQ-USB eval board and connected to my PC running with WINDOWS98 and running the Spark Fun Monitor program, it works fine but , if I initiate the IQ module with a factory reset, it quits working. Tech support person I talked to at Spark Fun would not tell me what parameters they are using to set up the IQ module. I would any help I might receive in operating the IQ module with the PIC16f627A operating at 4 mHz.

LCW

lcwengr:
I wrote a program to read NMEA data into the onboard USART.

.

.

I initialize the USART to transmit at 9600 baud and receive at 4800 baud .

How did you manage that, given that no PIC's USART supports separate transmit/receive baud rates?

I have a NAND switching circuit that is controlled by output bit RA1 of the PIC uP. This circuit selects which port of the IQ module feeds the PIC USART. The buad rate of the PIC USART is switched in accordance with the port input to the PIC.

LCW