Hi everyone , I’m trying to do a wireless comunication between two RF’s (TRF-2.4G exactly)
The first step is the configuration of the RF, but also i have to configurate the usart on the MCU.
I have to connect the RF to the pic with 4 pins to CE,CS,DATA,CLK1 and in case of reception mode DR1.
The MCU have RC6 and RC7 how pins for RX and TX… and i didnt use them (i use the port A RA0, RA1, RA2, RA3, RA4).
The normal configuration of the usart still works? I say, Can i do the configuration normaly without any changes?
Sorry, I’m new on this.I have this doubt for a long time, and i have to move on with my proyect. ![]()
Thanks for any help you can give me…
PD: i configure or i trying to configure the usart with the library usart.h of c18 compiler.
OpenUSART( USART_TX_INT_ON & //transmit interrupt on
USART_RX_INT_ON & //receive interrupt on
USART_ASYNCH_MODE & //Asynchronous mode
USART_EIGHT_BIT & //8-bit data
USART_BRGH_HIGH, 129) //Baud rate high and spbrg