I am trying to view my cam processed files for a project in Viewplot, but I keep getting an error “Can not load drill file with drill tools”. I set it as 2.4 with leading zeros and I am using the Sparkfun cam file with all the defaults. Here is my .dri and my .TXT if you see any errors.
.dri:
Generated by EAGLE CAM Processor 5.4.0
Drill Station Info File: C:/Documents and Settings/Kevin/My Documents/eagle/IMU/Mini PIC IMU .1.dri
Date : 3/4/2009 5:47:06 PM
Drills : generated
Device : Excellon drill station
Parameter settings:
Tolerance Drill + : 0.00 %
Tolerance Drill - : 0.00 %
Rotate : no
Mirror : no
Optimize : yes
Auto fit : yes
OffsetX : 0inch
OffsetY : 0inch
Layers : Drills Holes
Drill File Info:
Data Mode : Absolute
Units : 1/10000 Inch
Drills used:
Code Size used
T01 0.0200inch 23
T02 0.0276inch 5
T03 0.0400inch 23
Total number of drills: 51
Plotfiles:
C:/Documents and Settings/Kevin/My Documents/eagle/IMU/Mini PIC IMU .1.TXT
.TXT:
%
M48
M72
T01C0.0200
T02C0.0276
T03C0.0400
%
T01
X3181Y1985
X3681Y2005
X4181Y1985
X4681Y2005
X5081Y2645
X6307Y3425
X7581Y3995
X7981Y5095
X9281Y5395
X7981Y7095
X6081Y5195
X4581Y5345
X4081Y5345
X3631Y4945
X3781Y4495
X4531Y4345
X2831Y4095
X2881Y5395
X6681Y2295
X9281Y3395
X10231Y2395
X10181Y1845
X10881Y3595
T02
X1181Y4014
X1181Y4604
X1181Y5195
X1181Y5785
X1181Y6376
T03
X2031Y1595
X2031Y2595
X2181Y7745
X1181Y7845
X3181Y7845
X4181Y7745
X5181Y7845
X6181Y7745
X7181Y7845
X8181Y7745
X9181Y7845
X11181Y7595
X12181Y7595
X13181Y7595
X13181Y6595
X12181Y6595
X11181Y6595
X11181Y5595
X12181Y5595
X13181Y5595
X13181Y4595
X12181Y4595
X11181Y4595
M30