Troubleshooting the WiFly shield for Arduino

I’m a little confused about the relationship between Arduino and the WiFly shield. I’m developing an application to monitor my boat and most importantly the level of water, in case the automatic pumps stop working for some reason. It works as expected, but if I telnet into the WiFly the sketch stops running. If I reboot the WiFly, only the shield reboots, not the Arduino Uno. Do I really have to connect some kind of relay to the WiFly itself to be able to power cycle the whole thing and get the Arduino Uno to reboot and rerun the sketch?