True 3.3v LCDs

How about some 3.3v lcds? Ones that can run both logic and backlights off 3.3v. No need for any charge pumps or bias tricks.

www.topwaydisplay.com for example has LMB162ADC-4, which can operate within 3.3V voltage even the Backlight ( STN gray LCD and white LED backlgiht). Around $3.00 in qty of 200.

I’m sure there are others…

thanks.

I read on another forum that someone modified a Nokia 6610 LCD to use the backlight LCDs in parallel instead of series (The backlight is just 2 side-facing white SMD LEDs with a forward voltage of 3.3V and forward current of 20mA). As long as you had a 40mA current-limited 3.3V supply, you could run them off 3.3V. However, you may as well get a charge-pump since it saves you modifying the LCD.