First thanks for responding with help.
This is my initial order number: 7094257
When I first got the unit it was not working “no display” no bluetooth nothing they told me send it back to be repaired.
This was my RMA number: 28274
I received the following explanation:
"Our engineer has fixed your device. Here are his notes:
Testing Notes:
Looks reasonable from the outside. All parts are in kit.
Unit not low, charging at 1.6W. Unit will enumerate
Defective display board was causing I2C failure.
We will be shipping your part out on Thursday at the latest. We will get you a faster shipping method than FedEx home delivery, too. As the product was indeed inherently defective as you had described."
When the unit was returned the display, and bluetooth were working.
I was trying to get it setup as a rover to the base station I already have set up.
The issue I was having was that I could either get corrections in “Devoice accurate” or “output to swmaps” across the same bluetooth connection. if I tried to get both I was getting failed connections on swmaps.
So my thought was to do a reset to factory defaults i.e. from the main serial menu “s” then “r” then “y”
That appeared to put me in the condition I am now, Sorry but I would think setting something to defaults would not make it stop working. It did prompt me to put in a “y” confirmation>
“Resetting to factory defaults. Press ‘y’ to confirm:”
This say’s nothing about breaking, or making non functional.
I simply wanted to get it back to the condition it was delivered in so that I could go through the process of setting up as a rover with RTK corrections from my base. figuring I might have missed or messed up a step.
Anyways…
I was able to downgrade the firmware. process output follows:
"Uploading firmware
Command: esptool.main(–chip esp32 --port \.\COM6 --baud 921600 --before default_reset --after hard_reset write_flash -z --flash_mode dio --flash_freq 80m --flash_size detect 0x1000 C:\Users\root\AppData\Local\Temp_MEI147922\RTK_Surveyor.ino.bootloader.bin 0x8000 C:\Users\root\AppData\Local\Temp_MEI147922\RTK_Surveyor.ino.partitions.bin 0xe000 C:\Users\root\AppData\Local\Temp_MEI147922\boot_app0.bin 0x10000 C:/Users/root/Downloads/RTK_Surveyor_Firmware_v1_12.bin)
esptool.py v2.8
Serial port \.\COM6
Connecting…
Chip is ESP32D0WDQ5 (revision 3)
Features: WiFi, BT, Dual Core, 240MHz, VRef calibration in efuse, Coding Scheme None
Crystal is 40MHz
MAC: 30:c6:f7:41:4c:3c
Uploading stub…
Running stub…
Stub running…
Changing baud rate to 921600
Changed.
Configuring flash size…
Auto-detected Flash size: 16MB
Flash params set to 0x024f
Compressed 17984 bytes to 12318…
Wrote 17984 bytes (12318 compressed) at 0x00001000 in 0.2 seconds (effective 897.8 kbit/s)…
Hash of data verified.
Compressed 3072 bytes to 129…
Wrote 3072 bytes (129 compressed) at 0x00008000 in 0.0 seconds (effective 4098.7 kbit/s)…
Hash of data verified.
Compressed 8192 bytes to 47…
Wrote 8192 bytes (47 compressed) at 0x0000e000 in 0.0 seconds (effective 13113.8 kbit/s)…
Hash of data verified.
Compressed 1785392 bytes to 1132701…
Wrote 1785392 bytes (1132701 compressed) at 0x00010000 in 18.1 seconds (effective 788.9 kbit/s)…
Hash of data verified.
Leaving…
Hard resetting via RTS pin…"
System status output
"Menu: System Menu
GNSS: Offline
Display: Offline
Accelerometer: Offline
Fuel Gauge: Offline
microSD: Offline
MAC: 0000 - GNSS Offline
d) Configure Debug
r) Reset all settings to default
x) Exit"
system reset output
"
rst:0xc (SW_CPU_RESET),boot:0x13 (SPI_FAST_FLASH_BOOT)
configsip: 0, SPIWP:0xee
clk_drv:0x00,q_drv:0x00,d_drv:0x00,cs0_drv:0x00,hd_drv:0x00,wp_drv:0x00
mode:DIO, clock div:1
load:0x3fff0030,len:1240
load:0x40078000,len:13012
load:0x40080400,len:3648
entry 0x400805f8
Starting FS
SparkFun RTK Facet v1.12-May 3 2022
Reset reason: ESP_RST_SW
Display Error: Not detected.
MAX17048 not detected. Continuing.
I still have access through a USB console but I don’t see a way to setup wifi in this firmware.
I cannot get a display; nor does it show up as connectable on Bluetooth. Same as before the firmware downgrade to 1.12
Awaiting further instructions, and again thanks for all the help
Steve