uMiRF and MiRF V2 work together

Will the uMiRF and MiRF V2 work together? I’m building a wireless joystick and the joystick has no room for the MiRF V2 board with the antennea but I need > 50ft which the MiRF V2 w/ built in antennae doesn’t get, the uMiRF does get 60ft so thats good enough, but I already have 1 MiRF V2 with the antennae already so i dont want to have to buy 2 uMiRFS. Anyone got any ideas?

Yeah, they will work together with certain settings. There is a section in the 24L01 manual (the chip in the MiRF v2 board) that tells you what the settings should be to talk to a 2401 (the chip on the MiRF board).