And and and…
uMiRF (Micro-mirf) has the second channel fully brought out! The uMiRF will have the .1" header footprint for the basic, single channel access but will have three pins off in the corner for access to the other channel.
We will also have addtional functionality. The original RF-24G unit simply tied the PWR_UP pin to VDD. This pin is essential for low power designs. We successfully controlled it on the WiTilt board to get our system below a 1.2mA avg current with a 10Hz dual axis tilt reading.
The new uMiRF ties the PWR_UP pin to VDD via a 100k resistor. It is also accessable via a throughhole pin - though not inline with the normal .1" minimal header.
Finally - we are hoping to test the uMiRF with a SMD footprint. That is, the uMiRF module should be able to be soldered directly to a PCB rather than using a bulk .1" header.
All of this is merely preview until we have the units built, in hand, tested, and ready to go. Pictures are definitely worth a thousand words. The Chinese labor day is delaying all PCBs for 6 days. We should have all parts in 10-14 days. We’ll let you know The front page is always where the latest parts are announced.
Which reminds me - I think we have 3 new items for today… Jeesh.
-Nathan
Thought it best to un-hijack another thread ![]()
Looks pretty there, on that front page. I actually have a question about the design process. I’m considering a chip antenna over a PCB printed antenna, given my low rate production and lack of fancy test equipment. Was it easier to work with the chip antenna design? I’ve seen the Yageo antennas go for a bit under $5, so that’s worth a tradeoff of a square inch or so of PCB space if it can give me similar or better performance and easier implementation. and small size can’t hurt, either ![]()