Hello,
I’m pretty new to this space so please bear with me; my project involves a quadcopter with a Matek H743-SLIM flight controller running ArduPilot 4.4.0.
I’ve successfully connected GPS from the RTK2 board to the flight controller. A GPS signal is acquired and everything looks good there at the moment.
However I also noticed the SDA and SCL pins on the board and also wired those to the flight controller but the compass is not detected. My two assumptions are: (1) SDA and SCL designate the compass (2) the RTK2 board has a compass onboard.
I have another Holybro GPS RTK (w/ compass) and when I connect it to the same pins on the flight controller a compass is detected so it doesn’t appear to be an issue with the flight controller.
I attached an illustration of the wiring between the FC and RTK board.
Again, thanks for reading your patients and I’m beginning to step into this electronics space.