Good afternoon,
Let me picture the situation first. A device running with a arduino mega build in to a electrical box has a display (JHD1313M1) connected with about 1m of cable in between. Now it’s possible that the display starts doing strange things and my guess the issue is the lenght of the cable that’s likely affected by surrounding voltages up to 400v.
I tried to fix that with 2 qwiicbus endpoint boards and followed “Alternate 2 - VCC2 at 3.8V to 36V” from this guide https://learn.sparkfun.com/tutorials/sp … okup-guide because I need 5V to power the display so 3.3V is not sufficient.
on the arduino side I connected the obvious wires: 3.3v, gnd, SDA and SLC to the arduino and next to that connected a external stable 5V (not supplied by the arduino) to VCC2 and it’s GND to GND2.
on the display side I connected the SCL and SDA + the VCC2 and GND2 to the display.
Yet somehow the display is not showing the right things and insteed showing black squares on the top rop and is blank on the bottom row
When measuring voltage on the Display side i got 5V on VCC2 powering the display and a 3.3V on the 3.3v pin supplying the qwiicboard. Next to that i checked continuity on the SDA and SCL pins as well.
So far I have no clue what i’m doing wrong here.
https://i.imgur.com/k6LOEP3.jpg https://i.imgur.com/0M5wjhC.jpg