Hi! I would like to send picture to FTP server and i managed to send it but it gets very corrupted. In picture are missing segment of picture. Picture in module is saved correctly but when i try to send it, half of picture is good but another half is corrupted. For reading picture i’m using file.readlines()?
readlines() is completely inappropriate for use with a picture, as it breaks up the file into lines of text - even though carriage return/linefeed characters do not have any such meaning in most graphics formats. Use file.read() if you’re sure the entire file will fit into RAM; otherwise, use something like file.read(4096) in a loop to read it in chunks. Also, use mode “rb” instead of “r” when opening the file - I’m not sure if that’s absolutely required on the Telit modules, but it won’t hurt to explicitly indicate that you’re reading a binary file rather than text.
Hi! Tnx for the reply!I’ve try before the file.read(4096) in a loop like:
for line file.read(4096):
MDM.send(line,0)
but then data is sent “bit by bit” until it reaches the 4096 and it is to slow for my project, for 4096 size of data takes about 2 minutes to send to FTP server.I’m using always ‘rb’ = read binary
That’s not valid syntax; I assume you meant “for line in file.read(4096):”, which I’d expect to be horribly slow! The read method returns a single string, not a list of strings as readlines does; iterating over a string gives you characters, not lines, so you’re sending a single character at a time (and NOT looping to read additional blocks of data from the file). Try something like this:
while 1:
block = file.read(4096)
if not block:
break # EOF reached
MDM.send(block,0)
Finally fixed it!The problem was that while sending binary data of picture the data was lost during upload, so you have to check for the lost data and resend again binary data which was lost.