USB CH340 sparkfun edge

Please could this issue be escalated as I need further technical support?

tx

It seems I cannot upload, so USB/340 is almost certainly the issue.

ASB:

Failed to respond

Fail

Tries = 3

Upload failed

I believe SVL is not installed when product is shipped, but for completeness

SVL:

Phase: Setup

Cleared startup blip

Failed to enter bootload phase

Target failed to enter bootload mode. Verify the right COM port is selected and that your board has the SVL bootloader.

There are many articles on this forum about CH340 driver and the solution. Try a to do a search

EDIT : just saw the other post you did around the same topic. As the echo worked, the driver seems to be working.

Next to that with an EDGE there was often the problem that the upload sequence was not completely followed. (as defined on https://learn.sparkfun.com/tutorials/pr … or-success)

Press and hold the Reset button

While still holding down the Reset button, press and hold the 14 button

Release the Reset Button

Hit Upload in the Arduino IDE (or use your keyboard shortcut)

Release the 14 button (after the upload has completed)