Hi,
I’m looking for a chip that can handle both a USB CDC connection and also allow a USB memory stick to be inserted for data logging applications.
The CDC i/f would be used to configure the device, retrieve battery status, set logging parameters etc. The memory would then be inserted to the same port and be used to log data.
There are a couple of chips at Sparkfun that provide a USB memory i/f that use a SD card. As a stretch I might be able to use these, however space is limited and I’d have to use a MicroSD card…are these compatible?
I’m also aware that the new Microchip PIC32 range of microcontrollers have an OTG stack…but would prefer to stick with a lower spec 18F4550.
Any suggestions would be very helpful.
Phil