Hi,
I am working on a project and I am using Arduino Nano board. I have interfaced multiple sensors & modules with it, so I am out of all pins, I have connected a sesnor at Pin # 1 too, which is the TX Pin. IT works fine.
But when I connect a sensor with RX pin, it gives error in uploading code, when I remove that sensor it works fine.Once code is uploaded then pin works fine everything works gud.
Thing is I am working on a robot so I can’t remove pin everytime I need to upload code, it involves lot of testing.
So, is there any way to solve this issue??
I am using this[ Arduino Nano, to remove the confusion as there are many such simialr boards are present.
Thanks.](Introduction to Arduino Nano - The Engineering Projects)