Hello, I am sort of a beginner at dealing with electronic components and did not do due diligence before making a purchase. The project I’m trying to complete is using the DE2120 barcode scanning module with an ESP32 Wrover kit microcontroller. However, I did not purchase the breakout board that would let me power and use the pins on the barcode module. Is there a recommended way to still use the module with the ESP32? The ESP32 itself has a mating connector spot for its OV2460 camera module, and it is a 24pin FFC connector. I’m not super well versed and am not sure if the 12pin FFC with the barcode module would work with that. Would I have to remap the pins using a library of some sort?
Sorry for all the questions, any direction would be much appreciated.