Using a magnetometer and a clothes washer

Hi. I’m still a beginner, but I think I can learn enough for this. The number of LEDs (out of about 18 LEDs, unless 12 is a lot easier) that are on, and their color, will indicate how much a ray (that makes an angle, maybe from yaw, from a magnetometer, that is on a sleeve of a dance costume) is pointing towards a location (miles away from the dancer wearing it) that is important to the dancer. The LEDs will be connected to the costume using electronically conduction thread, as a wearable. Though I don’t know whether it is best, someone told me that, because I want to put the costume in a clothes washer and drier, to protect it from water and maybe heat (from the drier), I will need a removable module. The removable part of the module will be kept out of the clothes washer and drier while the rest of the module is in, and be reconnected (to the rest of the module) after the drier is done. But I haven’t been able to find such a removable module. I’ve only found an Adafruit FLORA 9-DOF part that is no longer stocked, and a STEMMA QT 9-DOF part, which I’m guessing won’t withstand the clothes washer and drier, but I’m only guessing.

Is crossposting allowed? This is a little different from what I posted in another company’s forum, a while ago. Thank you.

Check out our LilyPad products https://www.sparkfun.com/catalogsearch/result/index/?p=2&q=lily which are sewable and washable (with care!). Low temps, non-caustic soap

We also sell a kit with a lot of things together (I think you’d just need the accelerometer added)

Thanks, @TS-Russell

I couldn’t find the word “magnetometer” or “DoF” (degrees of freedom) at that page.

Is that the least expensive and simplest sewable electronics kit, for a beginner who has no experience with LilyPad, and who only wants to learn enough (and have enough) to do what I described, for now?

We don’t sell waterproof magnetometers…but you can try coating one with clear nail polish or similar; there is an accel (don’t search DoF)

Yep

Thanks again, @TS-Russell

I searched using “accel” and accelerometers showed up, so I’m guessing accel stands for accelerometer. Should I look more for one with a magnetometer? I may not understand.

I’d like to eliminate things that seem too good to be true:

  • What is an example of a removable module?
  • Will a stackable work? I think those are the boards that usually have both male (on the bottom) and female parts (on the top) around the edge. But maybe the part that stays on the fabric of the costume, while the rest stays out of the washing machine and clothes drier, should only have male parts (because male parts seem, to me, easier to dry than female).
  • Is my guess, that Qwiic won’t work, correct, even if the male end of the cable is on the fabric?

In the lilypad search I shared there is an accelerometer. Lilypad products are the only washable items that we sell; regular boards/sensors are not

We don’t have your ideal product, but we have enough stuff that you could very likely make it work with a bit of effort…

  • What is an example of a removable module?
    What do you mean, precisely? Most things are removable in my eyes

  • Will a stackable work? I think those are the boards that usually have both male (on the bottom) and female parts (on the top) around the edge. But maybe the part that stays on the fabric of the costume, while the rest stays out of the washing machine and clothes drier, should only have male parts (because male parts seem, to me, easier to dry than female).
    I’m only recommending LilyPad items for this, unless you apply a conformal coating

  • Is my guess, that Qwiic won’t work, correct?
    Correct…unless you hotglue the connections before getting wet and remove/replace each wash cycle?

Thank you, @TS-Russell. What type of effort?

I just asked for an example of one, where it was brought up, in the Arduino forum.

Sorry, right after you quoted it, I edited and saved the post you quoted.

I think the best way so far is to put a 9-DOF (magnetometer included) board at the bottom of a box and fill the box with epoxy potting, to make it waterproof. I was told making a vacuum chamber might be useful, but I’m not sure where (in the box) to put it, how to make it, or why. Adafruit FLORA sewable threads could be connected to the board, or wires connected to the male end of STEMMA, STEMMA QT, or Qwiic cable; I think. Right now, my biggest problem is with the way the threads will come out of the flat epoxy top. First, I want them to be perpendicular to the top. Second, the distance between any thread and the one it is closest to should be the same as the distance between any other two (that are closer to each other than any others, with the exception of if there is a thread on its other side). How do I do this? Or is there a better way than all of this? Thank you.

Are the two Js in the thread the same person?

I think the first priority should be to be a prototype without regard to washing survivability. It’s a big complication and I’d hate to give up early on the project for flat thread or epoxy reasons. Most costume items aren’t intended to withstand the rigors of machine washing.

That’s used to help suck air bubbles for more complete encapsulation. There are probably also curing and/or drying (thermal?) considerations for some kinds of reactions but mainly bubbles.

Yes, and notifications of your post went to two different email addresses. I’m still thinking about the rest of your post, thank you.

Thank you, I used these three parts, among others:

  • SparkFun PID 15423 Qwiic Micro - SAMD21 Development Board
  • Adafruit 9-DOF Orientation IMU Fusion Breakout - BNO085 (BNO080) - STEMMA QT / Qwiic
  • LEDs

It rarely worked for long enough, without the LEDs doing something unexpected, and then (after they did the unexpected thing) they stopped reacting/changing. But, for some reason, it finally worked for long enough for me to make a YouTube video of it.

I’ll get back to this topic, maybe about washing survivability. Please let me know if you have something more in mind.

I hadn’t realized you had already gotten it working, even if for only short times. Very cool.

You’ve probably already thought of ways to improve your proof-of-concept for durability and repeat uses. Refine with an eye toward eventual washing.

Thanks. Would someone please compare LilyPad, a conformal coating; and pot material (a special epoxy) on top of a magnetometer in a removable box, with female pin headers on top of the pot material; and other options (if there are any)? It would be removed before the rest of it is washing. I think LilyPad might be able to connect to the magnetometer in the box using I2C.

This is for the dance costume, that uses yaw from a magnetometer on a dancer’s limb to control what costume lights do, according to how much the limb points towards an important location. To help avoid compatibility problems, would you please help me find the chip family of FLORA - Wearable electronic platform - v3 (product ID: 659) at https://www.adafruit.com/product/659, such as by telling me whether there is a better way to search than using, “What is Adafruit FLORA platform v3 chip family?”

What do you mean by “chip family?”
That board is pretty much just the same as the LilyPad Arduino USB - ATmega32U4 Board.

Thanks for your question about chip families. The most useful way I can think of answering your question is with examples. The examples (I think) are in the picture, which is shown here, and is also at https://learn.adafruit.com/adafruit-9-dof-orientation-imu-fusion-breakout-bno085. Please let me know whether I should try to describe chip families more, though they are new to me too.

Ah, I see where you’re going with that question now.

The Adafruit board you linked has an ATMEGA32U4 microcontroller, it’s different than a SAMD, RP2040, STM or nRF based board and I don’t know how nicely it plays with a BNO08x but it’s worth a try.

Sparkfun does have a SAMD51 based board, the Thing Plus SAMD51. You could give that a try if the ATMEGA32U4 doesn’t work. The same Arduino libraries will most likely work with this.

The Raspberry Pi Pico is a RP2040 based board and super cheap, you might consider it as well but you might have trouble finding libraries for the part you’re wanting to use.

What would be the best board(s) to practice soldering with, so I can eventually solder a BNO085 (which is at https://www.adafruit.com/product/4754)? I don’t have any tools or much experience.

We have a few soldering kits meant for beginners, I’d probably look at this one heART - Surface Mount Soldering Kit because it uses SMD components

We also have https://www.sparkfun.com/sparkfun-weevileye-beginner-soldering-kit.html and https://www.sparkfun.com/lighthouse-beginner-soldering-kit.html which are fun too!

Another good way to practice is getting a bunch of 0.1" headers and a solderable breadboard. Just solder headers in row by row until you get good.