Hi! First post, I’m excited to see where this goes.
I have a wearable project I’m planning out, already have purchases most of the LilyPad components, but two issues have me stumped, relating to the LED lighting. I have 0 experience sewing, and only a bit of electronics experience, so I’ll need some guidance. I hope this is the right place.
The project is for LEDs (like https://www.sparkfun.com/products/12664) mounted onto a commuter backpack. The backpack is currently quite water-resistant with a lining and cordura.
PROBLEM 1: If I want all the electronics to be located INSIDE the backpack, how do I let the LEDs poke through without losing the waterproof quality of the backpack? What are my options? I’m open to learning any skill I might need, but I’ll need some guidance to figure out the best approach.
PROBLEM 2: From what I’ve learned, the LilyPad operates from around 3.7V to a max of 5.5 V 150mA. I"m not sure if this is enough power to draw the kind of luminosity I’m hoping to achieve. If I need to use a secondary power source to power the lights, while controlling them using the LilyPad arduino, what’s the simplest circuit that I could use to achieve this? And are there any considerations (such as resistance or other things I barely comprehend) that I should know about or educate myself on?
Sorry, I know experts hate these vague “I’m totally lost” questions, but ya gotta start somewhere, and here I am.
Thanks to all those who take the time to share their knowledge!
Tom