Hii,
Using two CC1101EMK, I need to make them communicate using OOK
modulation at 420 MHz. I use the SmartRF Studio to generate RF
settings that is put in a header file that is included in an IAR
Workbench project.
In the SmartRF Studio, I change the “RF Frequency” and “Modulation”
settings. Other settings are left unchanged.
It does not work as there is no data received!
Are there any other settings (e.g. X-tal frequency, Channel bandwidth,
RX-filterbandwith…) that need to be changed?
Thanks.