Hello everyone!
I am using the “Venus GPS with SMA Connector” and getting stuck on update rates…
What I wanted is to get the $VTG message at 10Hz, and also the $GSA but no need for fast update there.
I first sent a 0x08 command to only get the needed messages … this is OK
I changed the baudrate to 38400bps withe the 0x05 command… this is OK
Then I sent a 0x0E command with 10Hz (0x0A) configuration … this is NOT OK
The only thing I get is the NAV LED blinking faster, XORed 10times a second… so I guess the command has been set correctly but obviously, this doesn’t match my needs because I still get my GSA+VTG messages at 1Hz rate…
After scratching my head few minutes, I realized that the 0x08 command allows to set intervals from 1 to 255 seconds… but not lower… So my head is itching much more right now ![]()
What do I actually get at 10Hz with the 0x0E command?
How do you get speed information at a 10Hz rate?
Help would be appreciated
PS : there’s a mistake in skytraq’s NMEA messages description : $VTG, 3rd field, Speed in KM/h has this format 000.0 and not this 0000.0