My quest to create a submersible/waterproof gps has me wondering where I’ve gone wrong:
I bought both the Venus gps and the recommended Vtorch antenna with SMA connector (VTGPSIA-3). My plan was to encapsulate both GPS and antenna in a block of, well, encapsulant and have a piece of glass for the antenna to look out into the sky.
I attached the antenna to a small (2" x 2") piece of glass by applying epoxy around the edges of the antenna. I tested the GPS/antenna and everything worked 100%.
I then put the glass/antenna plus Venus gps into a small container with the glass firmly attached to the bottom of the container with wire leads from the gps extending up above the container. I then poured an encapsulant into the container.
I ended up with a block of encapsulant with wire leads out one side and the other side with the antenna facing out the glass ‘window’.
Everything looked good. No encapsulant got between the antenna and glass. All the leads are sticking out of the encapsulant just fine. BUT - the unit used to be really fast to pick up a signal. Now it can take minutes or won’t connect at all!
The Venus gps can still be programmed and sends out a signal. But it only sportatically picks up signal.
My questions:
-
it looks like the base of the antenna (radome part) might be touching the SMA connector, could the is be the problem?
-
would encapsulant somehow get inside the antenna and cause the problem?
-
is there a better way to make a gps/antenna waterproof (submersible to say 10 metres?)
Any/all feedback appreciated.