macpod:
The venus modules are sensitive enough to get a track indoors… with the right antenna, usage, and environmental factors. I know this after building my own all-in-one module (which I hope to interest sparkfun in after testing the second revision! :D)
Here is what SkyTraq had to say when I asked them about the poor performance of the sparkfun module/sparkfun antenna combo:
The SparkFun evaluation board should get position fix around
30seconds with normal active antenna (as attached) under open sky.
The active patch antenna you are using from SparkFun, I’m not sure
what kind of environment it is particularly tuned for. Patch antenna
performance is highly susceptible to the particular application environment
it is tuned for. You can test if placing a large sheet of metal underneath
the antenna improves reception, or put the antenna on a cardboard box away
from the metal sheet improves signal reception.
So…you can try their suggestions, or try another antenna. Skytraq pointed this one out to me ( I have yet to try it):
http://www.inpaqgp.com/Specification/Sp … 090227.pdf
or another one that matches the requirements of the module better.
Before you do all of this too, lets make sure you are using the module right… while the sparkfun antenna does take a long time to get a fix, I found it pretty stable indoors afterwards. Are you sure you:
-Are powering it at the correct voltage?
-Are providing it with enough current?
-Do you have the antenna oriented correctly? The ceramic part with the dot should be facing UP towards space at all times.
-Do you have the module near any noisy circuitry/devices? (i.e. big motors)
Edit: I’m curious where you were planning on putting this in the car now too 
I do have the dot facing up. The module appears to be working correctly. If I hang the little stub out the window, it gets a fix within a few seconds. If I move it 2 feet inside the window, it loses it. I mean, I can do this at will while watching the output scroll up the screen.
I’m using the basic 3.3 v output of an Arduino Mega. It appears to run it.
The Arduino is in reality part of a current measurement system for an electric car. The car is a replica of a 1957 Porsche Speedster and is mostly fiberglass. See http://EVTV.me. I’m using a couple of LEM HASS hall effect current sensors to measure current and integrate it over time to derive Amp hours out and amp hours in from regenerative braking to establish a State of Charge on the cells.
I want to derive Miles to Empty. My hope was to use the GPS to integrate speed over time to derive distance travelled. I can then use distance travelled with AH consumed to predict miles to empty. But if the GPS is going to be in and out, the whole plan rather fails.
The unit was to be placed under the hood in the forward part of the car. Lots of EMI from an electric motor in the rear of the car. But the hood of the boot is fiberglass. A normal stereo GPS works quite well with the antenna placed under this fiberglass hood.
The Venus module was described in rather glowing terms as the BEST module they had found. If it won’t work 2 feet inside a bay window area indoors, I can’t imagine it working reliably anywhere, unless I want to wear it on top of my head with the convertible top down.
Thanks for the antenna link. I will try it.
Jack RIckard