I’m wondering about two settings in the Unified Configurator desktop app for the WT/Tsunami. My installed version is 2.00 beta2.
On the Trigger Settings tab, within the Function dropdown, there are two options, Enc Vol1 and Enc Pitch1. I could not locate any information regarding them in the SFE forums, user guide, serial libs, or the Robertsonics site. What do these do, and how can they be used? Wishful thinking leads me to believe they could be inputs for position data from a rotary encoder.
I’ve created similar functionality of course via the serial libraries, by mapping the expected range from either an encoder position or pot value, but a built-in would be cool.
Thank you!