Tsunami WAV trigger board for DIY e-drum computer, lots of questions

Hi,

I just bought the board (wig-20636) and I have an STP32 development board (quick and 3.3V) that translates sensor inputs to MIDI signals. So far, so good. I’ve downloaded the WTconfig, the Tsunami2_19_20240407_v203m folder (yes, I want mono). I will have many questions, so I start this topic.

The first question is in the WTconfig. When I select ‘Tsunami mono’ as product, which I believe I want, I cannot chose ‘MIDI’ in the baud rate pull-down. It is greyed out. Also when chosing ‘Tsunami stereo’, I can only chose midi when selecting ‘WAV trigger’. Does that setting work with the tsunami, and how does it know I want mono?

Any input / tutorial is appreciated,
Best regards,

Hugo