Wav Trigger assign multiple files per trigger

Hi all,

I’m about to get a wav trigger for a project and would like to do the following:

I will be using 10 triggers, each corresponding to a file(most probably different nots from a music instrument).

How can I have multiple sets of instruments(say 3-4 sets of 10 files) and be able to switch between them? I see that one of the options in the Function tab is "Trig Bank Up). Does that mean that I can have 10 files with audio, 6 empty, then 10 with audio, 6 empty etc and every time I trigger this command the triggers will be using the next set whenever active?

I know that I could connect an Arduino via serial and have complete and easy control over everything but I would really like to keep this project on one board for a change:)

I believe so…just be sure to name the empty files in sequence, and it looks like you can’t skip around…but it looks like you can cycle them in order

Great, thanks for the reply:)

Hi Petros !

Did you manage to use the same inputs for several sounds ?

I’m trying (in vain) to do the same thing, hooking an old keyboard to the firts 13 analog inputs , and being able to have several set of sounds with the same triggers.