Is it possible to use the fade in, fade out, and crossfade feature WITHOUT using an arduino or the serial connection?
I’m looking to do something similar to this:
Trigger #1 = cues a track
Trigger #2 = cues a different track (crossfading from track #1 if currently playing)
Trigger #3 = stops all track (but fades out)
Thanks!
Isaac
(Using Wav Trigger with most recently released firmware, as of Dec 2019)
             
            
              
              
              
            
            
           
          
            
            
              Hi Isaac,
Unfortunately, I do not think you will be able to use the fade track function using just trigger inputs. There is no option using the InitMaker utility for setting a trigger’s behavior to fade a track, you can only do that using the “TRACK_FADE” command. Robertsonics’ [WAV Trigger User Guide has a full rundown on both the serial control protocol and all the trigger options.
The only idea that comes to mind to use that with an external//physical input would be to tie a button to another microcontroller and have that send the serial command to the WAV Trigger. It’s a bit convoluted but might help you find a solution here.](http://robertsonics.com/wav-trigger-online-user-guide/)
             
            
              
              
              
            
            
           
          
            
            
              Thanks for the quick reply!
Makes sense… I guess my project would probably be better with incorporating a micro controller anyway…
Thanks!