I use a Wave Trigger board as a small sampler to read incoming MIDI notes
from a musical project. All my notes are sampled stereo 16bits .WAV files
and stored on a 64gigs micro SD card that the Wave Trigger reads.
The 12vdc power supply is stable.
The firmware has been upgraded to v1.34 and
I do not exceed the board’s max 14 notes polyphony. Ok.
Now, here is my problem:
While playing incoming MIDI notes to the WT board I get Intermittent sampling ‘stepping notes’
in the song… It sounds like 20 notes played very fast and stuck together.
I attached a .MP3 file (.ZIP) that plays an external synth on left channel
and the Wave Trigger board on the right channel so we can hear
that the problem is only from the WT board. The external synth notes
are rock solid meaning the MIDI info is correct.
I started to suspect the lenght of my filenames and shrunk them
with no more than 7 characters like for example: 030-F#1.wav
But that didn’t cure the problem… Still some stepping intermittent notes
that insert in the played song…
Here is the wavtrigr.ini file information included on the SD card:
#MIDI 1
This file was generated by the WAV Trigger Init File Maker v1.20
It is only required if you wish to over-ride default settings. You
may add your own comments below this line →
Any one who actually had that problem ?
Thanks for your support.
Jean-Pierre Desrochers
Wave Trigger Board reading errors.zip (668 KB)