I was so excited to get my Weather Carrier board with ESP32 MicroMod today! I have worked through and read all the docs, etc on these two gems, and was hoping that the example applications would ‘just run’ when opened and deployed. Sadly, that appears not to be the case.
Here are the specific problems I’m facing:
In the MM_Weather_CB_Test.ino example, (well in all of the examples)
#if defined(ESP_PLATFORM)
int LED_BUILTIN = 5;
Causes a compiler error:
In file included from /Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/cores/esp32/Arduino.h:185:0,
                 from /var/folders/ns/44h75gxn0v95t1xj67pdfjqc0000gn/T/arduino_build_561788/sketch/MM_Weather_CB_Test.ino.cpp:1:
/Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/variants/esp32micromod/pins_arduino.h:72:22: note: previous declaration as 'const uint8_t LED_BUILTIN'
 static const uint8_t LED_BUILTIN = 2;
Ok, so that’s just the built-in LED, I can live without that.
But it gets steadily worse:
MM_Weather_CB_Test:41:5: error: conflicting declaration 'int G0'
 int G0 = 4;
     ^
In file included from /Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/cores/esp32/Arduino.h:185:0,
                 from /var/folders/ns/44h75gxn0v95t1xj67pdfjqc0000gn/T/arduino_build_123506/sketch/MM_Weather_CB_Test.ino.cpp:1:
/Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/variants/esp32micromod/pins_arduino.h:42:22: note: previous declaration as 'const uint8_t G0'
 static const uint8_t G0 = 15;
                      ^
MM_Weather_CB_Test:42:5: error: conflicting declaration 'int D0'
 int D0 = 23;
     ^
In file included from /Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/cores/esp32/Arduino.h:185:0,
                 from /var/folders/ns/44h75gxn0v95t1xj67pdfjqc0000gn/T/arduino_build_123506/sketch/MM_Weather_CB_Test.ino.cpp:1:
/Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/variants/esp32micromod/pins_arduino.h:39:22: note: previous declaration as 'const uint8_t D0'
 static const uint8_t D0 = 14;
                      ^
MM_Weather_CB_Test:44:5: error: conflicting declaration 'int D1'
 int D1 = 27;
     ^
In file included from /Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/cores/esp32/Arduino.h:185:0,
                 from /var/folders/ns/44h75gxn0v95t1xj67pdfjqc0000gn/T/arduino_build_123506/sketch/MM_Weather_CB_Test.ino.cpp:1:
/Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/variants/esp32micromod/pins_arduino.h:40:22: note: previous declaration as 'const uint8_t D1'
 static const uint8_t D1 = 27;
                      ^
MM_Weather_CB_Test:45:11: error: conflicting declaration 'const int G3'
 const int G3 = 17;
           ^
In file included from /Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/cores/esp32/Arduino.h:185:0,
                 from /var/folders/ns/44h75gxn0v95t1xj67pdfjqc0000gn/T/arduino_build_123506/sketch/MM_Weather_CB_Test.ino.cpp:1:
/Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/variants/esp32micromod/pins_arduino.h:45:22: note: previous declaration as 'const uint8_t G3'
 static const uint8_t G3 = 17;
                      ^
MM_Weather_CB_Test:46:5: error: conflicting declaration 'int G1'
 int G1 = 12;
     ^
In file included from /Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/cores/esp32/Arduino.h:185:0,
                 from /var/folders/ns/44h75gxn0v95t1xj67pdfjqc0000gn/T/arduino_build_123506/sketch/MM_Weather_CB_Test.ino.cpp:1:
/Users/davidgs/Library/Arduino15/packages/SparkFun/hardware/esp32/1.0.1/variants/esp32micromod/pins_arduino.h:43:22: note: previous declaration as 'const uint8_t G1'
 static const uint8_t G1 = 25;
                      ^
exit status 1
Essentially, it’s un-buildable and un-runnable. What am I missing here?
 Have only done the standard Blink sketch and the Wifi example thus far (had to install the official esp32 BSP in addition to the SparkFun MicroMod BSP for compiler to work?), what files did you end up editing to get this working, just the example .ino?
 Have only done the standard Blink sketch and the Wifi example thus far (had to install the official esp32 BSP in addition to the SparkFun MicroMod BSP for compiler to work?), what files did you end up editing to get this working, just the example .ino?