What is the recommended way to remove the SD card from ESP32S3 Think Plus?

Hello, if I just remove the card, disconnect the power source or unplug the cable connected to the computer while a program is writing data to it, will I corrupt the file or damage the card?

What is the recommended way?

It can corrupt them (similar to any other situation while writing to the card)

You can make removal safer by calling “SD.end” after writes; you could also flush after writes like so:

File dataFile = SD.open("/data.txt", FILE_WRITE);
dataFile.println(sensorReading);
dataFile.flush();  // Forces physical write (not just buffer)
dataFile.close();  // Always close files properly

You can also implement the SD card detect pin to trigger such

// Poll card detect pin or use a button sequence
if (digitalRead(CARD_DETECT_PIN) == HIGH) {
    SD.end();
    digitalWrite(STATUS_LED, HIGH); // Signal "safe to remove"
}

Thanks. Is “SD card detect pin” a pin specifically for the SD card or just any physical switch connected to the pin is called “SD card detect pin”?