Finally getting back to using my Postcard + Compatibility Shield and I have two very basic newbie questions:
- When the Postcard is in RTK Fix Mode (4), is the position being logged to the shield’s SD card the RTK Fix position or the GPS fix position?
- If it is the RTK Fix position, is it corrected to WGS84 (the default for GPS) or is corrected to the datum used by the Base (NAD83(2011)(Epoch 2010.00)?
The reason I ask is the the position logged on the SD card is different than the position logged in the SW Maps track and I’ like to understand why.
Thanks! Len