The BatchPCB bot doesn’t show holes, so this may be a non-issue.
It looks like it’s not repeating the Y coordinates after they’ve been stated once. All of the holes in this board are in three different “rows”. For example, the T03 drill is all in Y15500.
I will edit and reupload to see it that helps.
Actually, no edit is required. Here’s something from RimuPCB’s help file:
Modal Data
This option, when enabled, eliminates unnecessary repeating of X or Y co-ordinates from the file when moving horizontally or vertically and reduces the size of the file somewhat. This option should normally be enabled.
It appears that BatchPCB doesn’t like that option being enabled while Advanced Circuits doesn’t mind.
Thanks for the pointer!
Odd. ViewMate and GC Prevue show the holes as being about 10X the size of the PCB no matter what selections I choose.