When connecting WIFI
Happens on Esp32
About “Brown out detector was triggered”
Of the following 6 points
Which is the main cause?
Healed while improving the following six.
Is there anything else?
Question intent
When making a board
I want to use it as a reference for stable operation.
1, noise
Example: IC GND, where multiple wires should be wired, must be disconnected
-
I connected FAN etc. to the output. As a result, the current of the serial power supply became insufficient. It was over 260mA.
-
Because of the hand-assembled experiment, the ESP32 IC was supported by electric wires.
It was supposed to stand up vertically.
4, power supply plus GND wire is too thin, all examples
I have wired with multiple cores.
-
Pull up GPIO35-39, which is not internally pulled up, with a 10K resistor.
-
WIFI connection control series
It will be completed in 500ms
I tried to perform extremely short processing by hand in an environment vulnerable to noise.