I have just started using Eagle Cad.
I have designed a small board 25mm X 25mm and put 4 copies of it on a 50mm square board which I now want produced by Itead.
Itead require that I send gerbers for various layers
GTL Top Copper
GBL Bottom copper
GTS Top Solder Stop Mask
GBS Bottom Solder Stop Mask
GTO Top Silk
GBO Bottom Silk
TXT NC Drill
GKO Board Outline
Can you tell me which Eagle layer numbers correspond to the names Itead use GTO, GTS etc . I know its obvious that
Eagle layer one is the top copper and 16 is the bottom copper , but when I make the gerber for GTL do I just use layer one or do I also need to include other layers like 17 ( Pads) and 18 (vias)
and when I make the drill file do I just use 44 ( drills) or 45( holes) or maybe both?
If some one could tell me which to include for each layer that Itead require I would be grateful
Regards
Don