I recently got my last project produced from iTead and got the boards today. In Eagle I made sure to hide the tNames layer as it interfered with my silk screen. However when the boards showed up they printed the tNames layer! How do I keep this from happening next time? Thanks!
Here’s what I had made: http://www.computersandcircuits.com/?q=c-bb-psu I’m currently on version 8.2 as of today (made some minor changes after assembling a couple boards) I just haven’t updated my website yet.
I don’t know what that layer is in Eagle but you made the Gerbers, did you not check them in a Gerber viewer before you sent them?
Or did you use ODB++ etc?
BTW: I see you have no fusing on your board. Also your tracks could be thicker given it is a PSU - what sort of current is it providing?
No I did not check them in a gerber viewer before I sent them I now have ViewPlot and it shows that layer in there. I hid the layer when I ran the CAM figuring it’d not do what was hidden but I see I was wrong
It should be able to output 1.5A on 5V, 800mA on 3.3V and 1.5A on the adjustable (accoring to the specs from the regulators used). I’m not sure what you mean by no fusing though.
I think I figured it out. I used the iTead CAM job this time instead of the Sparkfun one I typically use. I ran it with the Saprkfun CAM and opened it in ViewPlot and it’s as it should be. I also made the traces thicker (0.032) and moved traced to give proper spacing as needed.