Hi,
I come here to explain my problem using the wifi shield Roving Network RN-XV.
So I have the following set : arduino uno + wifi prototype shield + Wifi Roving Network RN-XV.
After lot of tests, I found that the library provided by Sparkfun doesn’t work for wifi deconnection and reconnection automatically. So I used the following librairy: https://github.com/harlequin-tech/WiFlyHQ.
I use this system to post data on a personnal webserver. Everything works great during 15 to 45 min, once this time is spent the program blocks. In order to make it works again, I have to remove the power supply from the arduino (a simple push on the reset button doesn’t work). That’s why, I think it needs to empty the capacities. It is not a problem of memory leak on the Arduino, I already check that, maybe a problem of memory leak on the Wifi chip.
Below is my code :
#include <SPI.h>
#include <WiFlyHQ.h>
#include "Credentials.h" // Contains connection informations (ssid, passphrase)
WiFly wifly;
/************ variables ******************/
unsigned long timet  = 0 ;
unsigned long time;
unsigned long period;
const char *data = "data to send to the webserver";
void setup() {
    Serial.begin(9600);
  
    while (!Serial) {
        // wait for serial port to connect
    }
    wifly.begin(&Serial, NULL);   
}
void loop()
{
    time = millis(); //Returns the number of milliseconds since the Arduino 
    //board began running the current program. This number will overflow 
    //(go back to zero), after approximately 50 days
    period = time - timet;
    if (period>10000){
        // if the wifi is associated we try to send data
        if (wifly.join(ssid, passphrase) && !wifly.isConnected())
        {
            // If the connection to the server is Ok then we send the data
            if(wifly.open("data.egreen.fr", 80))
            {
                //Send data to the server
                wifly.println( F("POST http://data.egreen.fr/energy/create HTTP/1.1") );
                wifly.println( F("Host: data.egreen.fr") );
                wifly.println( F("User-Agent: Arduino/1.0"));
                wifly.println( F("Content-Type: application/x-www-form-urlencoded") );
                //wifly.println( F("Connection: close") );
                wifly.print( F("Content-Length: "));
                wifly.println(strlen(data));
                wifly.println();
                wifly.println(data);
                // Close the connection and desassociate the wifi
                wifly.close();
                wifly.leave();
                // reset period, set timet to the current millis() and reset wh   
                period = 0;
                timet=millis();
            }
        }
    }
}
/**
 * Return quantity of free ram
 */
int freeRam() {
    extern int __heap_start, *__brkval;
    int v;
    return (int) &v - (__brkval == 0 ? (int) &__heap_start : (int) __brkval);
}
Any help would be apreciate ![]()
THanks by advance,
Irwin