Hi,
I’ve been using my RN-XV for about a week now. I originally hooked it up and had it start in ADHOC
mode, I then used telnet to the device to have it assoc with my AP and was happy.
Today I wanted to connect to the boards UART ( pins 2 & 3 & gnd ) off the RN-XV. I connected a USB to Serial
cable to my laptop and connected to the RN-XV.
I used 9600 baud, no parity, 1 stop bit, no flow control.
It connects but I only get gibberish. I can see data being received by the terminal app, but I cannot
for the life of me get it to print readable characters. I’ve tried different settings as well as different
terminal apps …
I’m sure someone else has done this… The RN-XV is powered by battery. Works just fine via telnet
but not over the UART / serial. The reason this is a problem is that I want to send data from a sensor
that talks rs232 and expected to be able to connect the two, but I can’t seem to get basic comm going
using serial.
I’m using a UC232A ( http://www.aten.com/products/productIte … _no=UC232A ) with Win7.
I’ve tried putty (serial), teraterm pro and hyperserialport with same results. And yes, I can talk to other
devices using the above with the same settings 9600-8-N-1 …
I even updated to the latest f/w and did a factory reset with no luck…
Anyone using a usb-to-rs232 adapter to talk to your WiFly RN-XV ?
I will try a “real” rs-232 port, when I can… just hoping my uart isn’t defective.