hello guys i try to configuration the shield with this settings:
set wlan ssid ARDUINO
set wlan join 4
set wlan chan 1
set ip adress 169.254.1.1
set ip netmask 255.255.0.0
set ip dhcp 0
set ip protocol 1
set ip host 169.254.1.100
set ip remote 9000
set ip local 8000
save
reboot
Now my phone my computer ecc find the new network but i can’t do it nothing because i can’t enter.
I try the telnet comunication but doesn’t work ![]()
somebody help me?
i try this sketch but nothing
/*
#include "WiFly.h" // Include la libreria Wifly
Server server(80);
char ssid[] = "arduino"; //nome della rete wireless
int ledPin = 2; // LED pin
String readString = String(50); //stringa
boolean LEDON = false; //LED status flag
int pwm_a = 3; //PWM control for motor outputs 1 and 2 is on digital pin 3
int pwm_b = 11; //PWM control for motor outputs 3 and 4 is on digital pin 11
int dir_a = 12; //direction control for motor outputs 1 and 2 is on digital pin 12
int dir_b = 13; //direction control for motor outputs 3 and 4 is on digital pin 13
void setup() {
//Set pin to output
pinMode(ledPin, OUTPUT);
pinMode(pwm_a, OUTPUT); //Set control pins to be outputs
pinMode(pwm_b, OUTPUT);
pinMode(dir_a, OUTPUT);
pinMode(dir_b, OUTPUT);
WiFly.begin();
Serial.begin(9600);
Serial.print("IP: ");
Serial.println(WiFly.ip());
server.begin();
}
void loop(){
// Crea la connessione con il client
Client client = server.available();
if (client) {
while (client.connected()) {
if (client.available()) {
char c = client.read();
//legge la richiesta dal client
if (readString.length() < 30)
{
//salva i caratteri letti in una stringa
readString +=c;
}
//riporta la stringa su serial monitor
Serial.print(c);
//verifica che la richiesta sia terminata
if (c == '\n') {
//verifica se sulla richiesta è presente l'attivazione del LED
if(readString.startsWith("L=LED_ON", 6))
{
//led acceso
digitalWrite(dir_a, LOW); //Set motor direction, 1 low, 2 high
digitalWrite(dir_b, LOW); //Set motor direction, 3 high, 4 low
delay(1000);
analogWrite(pwm_a, 255); //set both motors to run at 100% duty cycle (fast)
analogWrite(pwm_b, 255);
LEDON = true;
}else{
//led spento
digitalWrite(dir_a, HIGH); //Reverse motor direction, 1 high, 2 low
digitalWrite(dir_b, HIGH); //Reverse motor direction, 3 low, 4 high
delay(1000);
analogWrite(pwm_a, 100); //set both motors to run at (100/255 = 39)% duty cycle
analogWrite(pwm_b, 100);
digitalWrite(ledPin, LOW); // set the LED OFF
LEDON = false;
}
// risposta al client
client.println("HTTP/1.1 200 OK");
client.println("Content-Type: text/html");
client.println();
//set background color
client.print("<body style=background-color:withe>");
//send first heading
client.println("<font color='red'><h1>Arduino Wifly Shield TEST</font></h1>");
client.println("<hr />"); //separatore a linea
//visualizza valore canale analogico 0
client.println("<font color='blue' size='5'>Analogico CH0= ");
client.print(analogRead(0)); //visualizza il valore della variabile
client.println("<form><input type=submit value=CHECK ></form>");
client.println("<hr />");
//visualizza link
client.println("<font color='blue' size='5'>Link: ");
client.println("
");
client.println("<hr />");
//controllo led via checkbox
client.println("<h1>Controllo LED</h1>");
client.println("<form method=get name=LED><input type=checkbox name=L value=LED_ON>LED
<input type=submit value=submit></form>");
client.println("<hr />");
// Gestione LED con pulsanti
client.println("<form><input type=submit name=L value=LED_ON> </form>");
client.println("<hr />");
//client.println("<form><input name=L value=0>Numero da inviare<input type=submit value=INVIA></form>");
client.println("<form><input type=submit name=L value=LED_OFF ></form>");
client.println("<hr />");
//visualizza stato del LED
client.print("<font size='5'>Stato LED: ");
if (LEDON)
client.println("<font color='green' size='5'>ON");
else
client.println("<font color='red' size='5'>OFF");
client.println("</body></html>");
//cancella la stringa per una nuova lettura
readString="";
//ferma il client
delay(500);
client.stop();
}
}
}
}
}
someone can help me?