WIG-12772 Question

Hello, how much is the maximum sampling rate for WIG-12772?

https://learn.sparkfun.com/tutorials/lo … okup-guide

Frequency

The “Frequency” field only applies to ADC logging mode and is responsible for setting the sampling rate of the Logomatic. The number shown (100 in this case) is in Hertz and can be set from 1 to 9999. However, if the frequency safeties are active, the maximum values will be imposed as indicated in the Safety On section.

So is the max sampling rate 9999 Hz?

It would appear so.

Do you know any datalogger that is either Analog or digital input and has max sampling rate log of 2Mhz?