Working code for SCP1000 and Atmega128

Hi,

Does anyone have some working code which interfaces with an SCP1000 as a Hex that I can download into my Atmega128 to see if my SCP1000 is dead or not?

I can’t get my Bascom AVR code to work, but since at some point I am pretty sure I gave the SCP1000 a taste of 5v on one or more of the pins I don’t even know if the sensor works anymore!

What are the chanes I toasted it?

Kind thanks,

Serge

chances are good it will survive if connected not longer than a few minutes.

SCP has zeners built-in on input lines.

however they are chances it became innaccurate by a percent or so.