Hey guys,
comparing schematics of boards
WRL-17743
and
WRL-20168
I find first has R8=100k resistor, latter R8=10k.
I want to use a switch to turn off the device completely when powered from battery.
I would like to have the battery permanently connected for example to load it if USB is plugged in automatically without need to switch on the battery power.
So I thought using the EN-pin, but current is a bit high to use it that way:
If I pull down the EN-pin next to R8, this would result in a current flow of roughly
WRL-17743 → I=U/R=5V/10k=0,5mA
WRL-20168 → I=5V/100k=0,05mA
First is quite much and a battery of 500mAh would discharge in ~41days, where with the 100k resistor it would last more than a year.
Why did that change? Was it intentional? How would I connect a battery to the system permanently, load it, monitor it and not discharge in about a month.
Maybe the board can be improved in that regard…
Best,
Michael