I recently bought an xbee retail kit (2 xbee modules, 1 xbee arduino shield) and an ardiuno pro 328. I soldered headers through the xbee shield and into the arduino pro and setup my USB module.
According to most tutorials I should immediately be able to send serial text and have the xbee/arduino send back the same text but this didn’t work. I then tried to upload a simple ‘blink’ test example, but I get an error code:
avrdude: stk500_getsync(): not in sync: resp=0x00
avrdude: stk500_disable(): protocol error, expect=0x14, resp=0x51
I’m getting signal to the xbee shield because the RSSI light comes on when I try and upload. Nothing else seems to flash on the arduino pro.
Note: after re-flashing the shield xbee using X-CTU (while mounted on the usb module) I eventually saw the DIN light flash indicating data was being received, but still nothing sent back.
Hmmmm… I’ve run around forums all over the web and tried various bug fixes including:
Trying with different baud rates, including the default 9600bps
Trying with the UART / DLINE switch at different states (and different baud rates).
Flashing the shield mounted unit using X-CTU (Modem:xbee 24 , Function Set 802.15.4)
Flashing the usb mounted unit using X-CTU (Modem:xbee 24 , Function Set 802.15.4 USB Adapter)
Double checked my soldering points, definately no joining areas, although I have soldered on the underneath side of the arduino pro and not the top (is that ok?)
I’ve ordered a UART > USB cable to see if I can flash the xbee on the arduino pro, and maybe upload some basic sketches. But am I missing something here?
This unit is really badly documented by digi.com, they don’t even have basic setup procedures for the arduino
. FYI the modem type (xbee 24) is not stamped on the unit or retail kit page on sparkfun. xbee s1 does not appear in the x-ctu list of devices. But thats what was detected using x-ctu.
Help appreciated. Apologies if I’ve left something out!
Windows 7 64bit (x-ctu seems to work ok even though its 32bit).
Arduino pro (new)
Xbee retail kit firmware version 10E8
9v batter powered