HELLO
I try, i try, … but nothing happen…
I am having issues with Sparkfun Xbee Shield ( http://www.sparkfun.com/commerce/produc … ts_id=9841 )
I want to communicate with 2 Arduino UNO, 2 Xbee Pro 60mW 802.15.4 (last firmware) ( http://www.sparkfun.com/commerce/produc … ts_id=8710 ), and 2 Xbee Shield Sparkfun.
I can configure the Xbee with Xbee Explorer (sparkfun) and X-CTU (that’s the BEST PART !!
)
They respond and i can change the setup, but i leave the basic setup, i was told that they should work with it, without any change.
With the Xbee explorer, i can see the Tx led blinking when i send something in the terminal, So I suppose the Xbee is working good.
I loaded the sketchs to simply communicate onto the UNO, (the one here http://arduino.cc/en/Guide/ArduinoXbeeShield ) and the board seems to do there job (at this point, no Xbee activated)
But when i unplug de USB cable and put an external power, and the Xbee On, the boards are working, but no communication at all between them !!
I tryed many thing, many configuration, tested many code on forums… and change the switch UART into the 2 positions on the Xbee SHield, but nothing happen.
I only have 1 Xbee Explorer USB, so i can’t test the communication without Arduino.
It seems that my setup = UNO + Xbee Shield + Xbee Pro 60mW don’t Work at all !!!
Plus, the Xbee Shield cannot be perfectly assembled on the UNO, it touchs the USB port. You can see this on this pictures :
http://yopayet.free.fr/arduino/XbeeShield3.jpg
http://yopayet.free.fr/arduino/XbeeShield4.jpg
I think there is a problem with Xbee Pro 60 mW and your Xbee Shield, and maybe with the UNO itself.
Don’t you think ?
The fact that the shield can not be closed to the Arduino may be the problem ?
Or the Xbee Shield is not made for new Arduino UNO ?
Please, help, it’s urgent for me i have to build something as soon as possible.
thk U.