I have XBee 1mW chip antenna module, I am using X-CTU. After typing +++ when I type ATND I get “ERROR” message. I couldn’t figure out why this is happening and I am also kind of rookie at this XBee stuf. What can I do to make ATDN work?
Channel and PAN ID parameters are the same on all modules I want to scan with XBee
The firmware version is the best way to ID your XBee modules and what Protocol is being used. You can get this by clicking on “Test/Query” in the PC Settings tab of X-CTU.
After typing the +++ do you get the ‘OK’ response? If not then the XBee didn’t see the +++.
Ok, you have Series 1 XBees with the latest 802.15.4 firmware.
Do other AT commands work? Like ATIS.
Are your other XBees powered on and connecting, Associated?
I’ll guess you are running these as Peer-to-Peer and not with one module set as a Coordinator. If this is true then I suspect that the ND command is not valid in Peer-to-Peer. Look in the doc starting on page 15 (XBee®/XBee-PRO Networks).
You could try setting one XBee to be a Coordinator, cycle power on all units and retry the ND command.