Hi all,
so I got the XBEE as I was told it was the simplest rs232 cable replacement out there, straight swap even. Anyhow, after trying every possible configuration I could, I get communication without precision.
I am passively monitoring my com port to see the communication, first off, it seems some of the data I am transmitting from the computer to the XBEE is bouncing back to the computer, sometimes characters are straight duplicated or received with extra/irrelevant characters in addition (and sometimes not). Also, the timing is off, by the time it sends the data sometimes my program will just say connection timed out.
I am using a XBEE connected to the computer with XBEE explorer, the device connected to the other XBEE ONLY uses the DIN and DOUT (TX/RX) transmission. I have been using this device with cables on 9600 8N1 perfectly; I have checked all my baud rates and even tried different ones. I have tried default settings on the xbees, 64 bit addressing (leaving MY=0) on both xbees, using MAC addressing with MAX header, with and without ACKS, etc. and NOTHING will clean up this sloppy communication I’m getting. I have tried messing with the virtual com port settings, etc, etc. The most useful setting I changed was the packet timeout, which I put to 0 so that the xbee does not wait to send any communication to one another, this resulted in the device not timing out the program when it is trying to download, but it is still impossible to download because the password is always sent incorrectly, yet is very close sometimes (I shouldn’t know this, but as I said, it will bounce back what it has received). Both devices are put as “END”… Im about to stomp on these things they are driving me crazy.
So I wonder, WHY does it seem that the XBEE Im trying to speak to is bouncing back the data packets? The only setting I never enabled was data collision prevention, and the two xbees are within a foot of each other using full power… is this a possible culprit? I wouldn’t think so since I also used 64 bit addressing.
XBEES IM USING:
XBEE SERIES 1 (XB24)
FIRMWARE: 1084
PLEASE, any help is appreciated! I was depending on these darn things, now they’re stinging me in the butt. :lol: