Xbee Pro Problems

hello i got 2 axe210 boards everything worked perfectly with normal xbee modules.

i used picaxe editor and x-ctu V.5.1.4.1 to edit module parameters i was able to control them whit picaxe, pc and with xbee standard I/O pins.

everything working perfectly but the problems arrived when i needed to use xbee pro modules for my project because iam doing a remote boat control and need around 1 mile range.

i replaced the le330 linear transformer from the axe 210 board whit a 800ma one. and the modules worked OK the problem was when i edited the module parameters and pressed write, it start working normally but gave a error on end and i cannot communicate whit the modules anymore. the light status still flashing normally on the board but cant restore the default settings or do anything to the module.

is not the baud rate since i have tried all of them and was using the default one so.

any ideas for a solution ???