20 days ago I acquired four XBee pro, on a XBee installed the firmware of coordinator, the other three as device / router, I tested and works perfectly, but the distance Indoor / Urban reaches about 30 meters and Outdoor line-of- sight reaches about 100 meters. What should I set up or should I make the XBee to reach the distances that say in the technical specifications of 100 meters in
Indoor / Urban Outdoor and 1600 meters in line-of-sight??
I think that the range specifications given are the best available from the family, and that installing a different antenna can change this performance.
For example, if you have the type with the U.FL connector and use a 15 dB panel antenna on each end, you can probably go several kilometers, well beyond the ‘maximum’ range. If you don’t mind exceeding transmission power limitations, throw a 24 dB dish antenna on each end and octuple the range.
If you use the built on wire antennas, and they are aligned so that their gain patterns (for dipoles/straight wires think of this as a flat disc extending from the sides of the antenna) allow a good link between the modules.
If you use the chip antenna, or don’t line up the gain patterns, I’m sure you can get very bad performance
Giving a ‘range’ on an RF device is subject to a lot of factors, and unfortunately the Xbee modules are rather optimistic in their assessments - not lying, just optimistic.
20 days ago I acquired four XBee pro, on a XBee installed the firmware of coordinator, the other three as device / router, I tested and works perfectly, but the distance Indoor / Urban reaches about 30 meters and Outdoor line-of- sight reaches about 100 meters. What should I set up or should I make the XBee to reach the distances that say in the technical specifications of 100 meters in
Indoor / Urban Outdoor and 1600 meters in line-of-sight??
Thanks a lot
Antennas, antennas, antennas. At least one end needs to have lots of gain. Either a gain omni (such as 8-12dBi) or a patch/yagi with gain that’s horizontal and not an omni. Lots and lots of antennas. Need to have XBee with U.FL antenna connector. Any 2.4GHz band antenna will do, such as