My XBee-PRO ZNet 2.5 modules have some serious issues.
I have one ZNET 2.5 COORDINATOR AT (1047) and three ZNET 2.5 ROUTER/END DEVICE AT (1247).
For some reason the end devices will only recieve (or send) data from the coordinator right after I program them. It’s like they don’t fint a network any longer. If they are without power for some minutes they stop working and I have to factory restore and then reprogram them again using the X-CTU software.
I will use this setup ten times, so I have tried this with 10 COORD and 30 ROUTER/END DEVICES and they are all showing the same behaviour.
The only connections I use are Vdd (3.3V), DIN, DOUT and GND.
Do anyone have any idea to what the problem might be?